VBUS.INRUSHOFF
Description
This parameter returns the voltage at which the DC bus inrush relay opens.
Examples
Usage
The drive configures this parameter based on power electronics component ratings. When the measured DC bus voltage VBUS.VALUE is less than VBUS.INRUSHOFF, the drive opens the inrush relay.
Context
For more information on DC bus operation, refer to Power.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-02-03-000 |
General Information
|
Type |
Read Only |
|
Units |
VDC |
|
Range |
N/A |
|
Default Value |
N/A |
|
Data Type |
Integer |
| See Also | VBUS.VALUE, VBUS.INRUSHON |
|
Stored in Non-Volatile Memory |
No |
Variants Supported
All variants supported.
Fieldbus Information
|
ID |
Instance |
Attribute |
Name |
Data Type |
Access |
User Mappable |
|---|---|---|---|---|---|---|
|
2505 |
1 |
2505 (0x9c9) |
VBUS.INRUSHOFF |
Unsigned16 |
Read Only |
Yes |
|
Parameter |
PNU |
Data Type |
Access |
Units |
|---|---|---|---|---|
|
VBUS.INRUSHOFF |
2505 |
Unsigned16 |
Read Only |
- |